During drive operation the drive display shows the following codes depending on the drive status.
Left Display (DriveControl device for regulating the speed, torque and position of a motor LED):
|
Display Code |
Status |
|---|---|
|
Powered on and FPGA"Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable" loading. If the display is locked on this code then operational and resident FPGA images are corrupt. |
|
Resident loading. |
|
Resident completed and waiting for the operational to start. |
|
|
Normal operation, position mode, no faults. |
|
|
Fault (see Fault and Warning Messages). |
Right Display (Controller LED):
|
Display Code |
Status |
|---|---|
|
Powered on and FPGA loading. If the display is locked on this code then operational and resident FPGA images are corrupt. |
|
Boot sequence. |
|
Resident completed and waiting for the operational to start. |
|
|
Operational - program not running. |
|
|
Fault (see Fault and Warning Messages). |
|
Copyright © 2015 Kollmorgen™ |
|